Press – 22.01.2016

Additional product ranges

NAVITIGHT® – the end of “cross-threading”

Manual screw fastening or trying to fasten a screw in a tight space can often result in the screw being tightened at the wrong angle.

Screws then become misaligned in the component (so-called “cross-threading”) and can jam. The result: damage to and even destruction of the holding thread. This can lead to manufacturing stoppages and considerable remedial costs.

This product is made by Böllhoff

 

Reliable screw fastening

The technical solution is as simple as it is ingenious. Developed originally for the automobile industry, NAVITIGHT® is now used in many other branches thanks to its outstanding properties. NAVITIGHT®’s secret can be found in the geometry of its thread run-out: the outer diameter of the narrower screw tip is smaller than the core diameter of the nut thread. The thread pitch, however, remains constant. When tightening the screw, the design brings the screw and nut into perfect alignment, ensuring that the screw fastening is completed correctly.

The optional additional paint removal function on the NAVITIGHT® screw will also help avoid other potential issues. In order to streamline processes, entire components are often painted in one go. This results in paint covering the thread which can lead to incorrect screw fastening. The NAVITIGHT® screw with paint-removal groove makes the internal thread viable once more as the groove scrapes the paint flakes from the thread.

Product benefits:

  • Prevents of incorrect fastening
  • Reliable screw fastening
  • Time and cost savings thanks to lower error rate
  • Possibility of automated screw fastening
  • Optimal angle results in minimal discomfort when screw fastening manually
  • Paint removal function ensures paint or other residues are removed from the mating thread

The standard NAVITIGHT® screw has a hex flange head and comes in sizes M 5 to M 14. Other drive forms and dimensions are also possible.

 

© Böllhoff Group, Bielefeld 2016

Reprint authorised.

 
 

Please send sample copy to

BÖLLHOFF CIVATA TICARET LTD. ŞTI
Ezgi Simsek
Internal Sales Engineer
6. Sokak No. 4 34953 Tuzla Istanbul
Mermerciller Organize Sanayi Bölgesi
E-Mail: esimsek@bollhoff.com

Downloads

For jounalists: related downloads.

If you would like to write about us, just download the press release and press photos.

Title Language Version File Download
Press text
.doc / 1.869 characters* January 2016 17 kB / ZIP
.doc / 1.869 characters* January 2016 17 kb / ZIP
Press photo (1)
.jpg / CMYK / 300 dpi January 2016 2569 kB / ZIP
.jpg / CMYK / 300 dpi January 2016 2569 kb / ZIP
Press photo (2)
.jpg / CMYK / 300 dpi January 2016 1614 kB / ZIP
.jpg / CMYK / 300 dpi January 2016 1614 kb / ZIP
Press photo (3)
.jpg / CMYK / 300 dpi January 2016 1924 kB / ZIP
.jpg / CMYK / 300 dpi January 2016 1924 kb / ZIP

* including blanks