eShopSearch
Country and language
Choose country:
Choose language:

Success stories

Signature Hiller

The German company Signature Hiller, pioneer in the signage sector, uses our RIVSET® self-pierce rivets in the production of motorway and road signs.

Freeway at night

Signature Hiller – the signature for quality in sign manufacturing

The German signage pioneer Signature Hiller uses our RIVSET® self-pierce rivets in the production of motorway and road signs.

Initial situation

The production of large signs

For the production of large motorway and road signs, first aluminium plates are cut to size and braced by means of oblong profiles on the rear. The reflective sheeting produced by use of a modern digital printing method is then bonded to the sign. The individual segments are transported to the motorway where they are joined.

Traffic signs are made from aluminium because it is a lightweight and durable material. The large dimensions of motorway signs, however, quickly result in larger weights. Originally, weld studs were used to be able to join the stiffening profiles on the rear to the aluminium material.

Later, when the innovative composite material DIBOND®traffic was used, a new generation of traffic signs was born. As the inventor of the original aluminium composite sheet, the 3A Composites Company based in Singen, Germany, makes a great contribution with the DIBOND®traffic. With the innovative composition of two aluminium cover layers and a laminated polyethylene core material, the sheet convinces through its suitability for lightweight construction, weathering resistance and its equivalence with a solid sheet.

The challenge: DIBOND®traffic is not suited for welding. This is where Böllhoff offers the perfect solution with RIVSET® self-pierce rivets.

Motorway signs
Sign productionSignature Hiller GmbH

Solution

RIVSET® self-pierce riveting technology – high strength and high process reliability

RIVSET® self-pierce riveting is a joining method to create mechanical high-strength joints from similar and dissimilar materials. Joints can consist of two or more layers.

In one step, the semi-tubular rivet punches through the top material layers, forms an interlock in the bottom material layer and also forms the characteristic button. The bottom material layer is not punched through so that a gas- and liquid-tight spot joint is created.

RIVSET® self-pierce riveting
RIVSET® self-pierce rivetingthe rivets
RIVSET® self-pierce rivetingSetting process

Result

RIVSET® „Roadsign”: robust and flexible self-pierce riveting system for modern sign manufacturing

From the beginning, Böllhoff had been involved as the joining technology expert. During numerous tests in the in-house joining technology laboratory, the RIVSET® self-pierce rivet proved to fulfil the high requirements for the joint. In combination with the RIVSET® “Roadsign” processing system, a self-pierce riveting system which had been especially developed for the manufacture of traffic signs, it was verified by the TU Dortmund University and approved by the German "Güteschutzgemeinschaft Verkehrszeichen und Verkehrseinrichtungen e.V." for the quality assurance for traffic signs.

Customer benefits

  • Flexible in use
  • Cost-saving
  • High quasi-static and dynamic strength

Product characteristics

  • Joining of dissimilar materials
  • No pre-punching
  • Particularly suited for hybrid joining
robust and flexible self-pierce riveting system for modern sign manufacturing
RIVSET® „Roadsign”robust and flexible self-pierce riveting system for modern sign manufacturing
A RIVSET® self-pierce rivet joint on a street sign by Signature Hiller
High-strength joint with RIVSET® self-pierce rivets

More Information

we will be happy to help

Do you have any questions or a current project?

Just let us know and we’ll get in touch

Contact us