Search
Country and language
Choose country:
Choose language:
Apply

Success Stories

RECARO Aircraft Seating

Pathbreaking solutions for seating systems above the clouds

Image of a business class seat from RECARO illuminated

ONSERT® flies business class

With the aim of reducing the weight of the CL6720 business class seats and making the processes more efficient, RECARO Aircraft Seating has developed together with the joining expert Böllhoff and DELO Industrial Adhesives an innovative solution based on the ONSERT® process.

Initial Situation

New challenges for developing leightweight business class seats with higher-level quality

Lightweight construction is an important goal in every segment of the aerospace industry – including cabin equipment. In addition, higher-level quality requirements for materials and processes have to be fulfilled. This also presented RECARO Aircraft Seating with new challenges when developing the CL6720 business class seats. A large number of electrical connection cables are hidden within a business class seat. These supply, for example, the in-flight entertainment, lighting or other control panels for the passenger. So quickly up to 100 holding points are required for cable and wire fastenings, which have to be fastened to the interior seat paneling made of composite material. The installation is traditionally done with inserts; they are bonded into the composite components by means of the potting process.

Image of a RECARO business class seat CL6720
The business class seat CL6720

Solution

ONSERT® Smart

With this ONSERT® version, the ONSERT® Smart basic element made of transparent plastic is bonded to the customer component with light-curing adhesive. The plastic and the adhesive meet the requirements of FAR Part 25, § 25.583 (60 seconds vertical burn)*. Especially the short cycle times, the material-friendly process and the design freedom of the fastening elements should be emphasised. The ONSERT® elements are processed manually by using the battery-operated ONSERT® Portable Mini.

Due to its modular structure, it is very well suited for use with restricted access to the adhesive area. After the base element has been bonded, diverse cable holders can be clipped on. These cable holders are available in different heights for different cable diameters, can be rotated flexibly and save weight. Thus, the cables do not come into contact with the seat lining during a flight, prevent static charges or damage to the cables and ensure safe energy management. With a term of 7 years, 122,000 ONSERT® Smart will be installed in the business class seats every year. Further dimensions are currently in the test phase.

ONSERT® Smart for cable management
ONSERT® for cable management in the aircraft
ONSERT® Portable Mini Battery-operated manual installation tool

Result

Cable management with ONSERT® Smart

Customer Benefits

  • After exposure immediately full mechanical strength
  • Short curing times (< 4 seconds)
  • Weight reduction through an all-plastic solution
  • REACH and RoHS compliant
  • Qualified and tested materials
Bonded ONSERT® Smart for cable management
Bonded ONSERT® Smart for cable management

Information and more

Downloads

Are you interested in ONSERT®? Please download further information here.