Press – 2016-12-19

RIVKLE® blind rivet nuts and studs

New battery setting tool for RIVKLE® blind rivet nuts and studs

The RIVKLE® B2007 is adding to the well-established Böllhoff tool range.

This new battery setting tool is made for demanding production challenges. RIVKLE® steel and aluminium fasteners from M 3 to M 10 can be processed with this cordless tool. Stainless steel fasteners can be processed from M 3 to M 8.

This product is made by Böllhoff

 

This is electro-hydraulic technology for high power at low weight. Up to 800 riveted joints can be realised with a fully charged lithium-ion battery. Moreover, the new quick-change system allows to change the exchange units without the use of a tool.

The B2007 has an ergonomic handle which is comfortable to hold and is also provided with shock protection. It is easy to use since only one button is used for operation – during the entire riveting cycle. The menu-based user interface on the LCD indicating riveting force setting, parameterisation of the riveting cycle and the battery state of charge makes this tool a great offer.

This setting tool was developed in close cooperation with Böllhoff customers to ensure very user-friendly handling in demanding industrial environments.

The advantages – an overview:

  • Range of use 3 kN to 22 kN (M 3 to M 10 RIVKLE® steel fasteners)
  • High capacity – up to 24 RIVKLE® fasteners/minute
  • Up to 800 riveted joints with a fully charged battery
  • Force control and direct input of riveting force

The tool comes in a case with operating instructions, a battery charger and one or two batteries. The exchange units (mandrel and anvil) as well as further accessories are separately available.

RIVKLE® B2007 battery setting tool

RIVKLE® B2007 battery setting tool

 

© Böllhoff Group, Bielefeld 2016

Reprint authorised.

 
 

Please send sample copy to

Böllhoff Group
Corporate Marketing
Anja Felsch
Archimedesstr. 1-4
33649 Bielefeld
Germany

Downloads

For jounalists: related downloads.

If you would like to write about us, just download the press release and press photos.

What? File format / characters Release date Type / Size Download
Press text
.doc / 1,590 characters* December 2016 18 kB / ZIP
.doc / 1,590 characters* December 2016 18 kb / ZIP
Press photo
.jpg / CMYK / 300 dpi December 2016 2204 kB / ZIP
.jpg / CMYK / 300 dpi December 2016 2204 kb / ZIP

* including blanks