Industry solutions

KTM Sportmotorcycle

"READY TO RACE" – for KTM these three words are more than just a slogan. They are a philosophy. With the ECOSIT® RFID Bin system we help to ensure that KTM is always ready to go.

Always ready to go

With the ECOSIT® RFID Bin system, we were able to speed up the logistics and procurement processes.

Especially at times of fluctuating demand, the efficiency of the procurement system really counts. We have found an innovative solution that is a perfect fit for KTM's dynamic business philosophy.

Initial situation


Making procurement more dynamic

It's all about performance. Over 200 world championship titles for riders of KTM racing bikes are no coincidence. Racing is the perfect environment for testing out and fine-tuning the latest equipment and technology innovations under extreme conditions. The insights that KTM has gained in motor racing have also been carried over into series production. Every motorcycle can be regarded as a blend of top-quality and thoroughly tested components. Every detail counts. This is true for the management of C-parts too. KTM is fast, dynamic and "ready to race" – so what could be a better fit than our ECOSIT® RFID Bin system?

Customer profile

Motorcycle manufacturer

Mattighofen, Austria





Switchover to the ECOSIT® RFID Bin distribution system

As soon as the weather starts to cooperate in spring, the motorcycle season gets going. From nought to one hundred. To help it respond better to seasonal fluctuations, KTM opted for our ECOSIT® RFID Bin system. This system also makes it much easier to take account of the constantly changing models of the various motorcycles.
KTM is seeing the benefit of the quick and easy order initiation process and the system’s short response times. With the ECOSIT® RFID Bin system, all relevant data necessary for prompt delivery is stored on the RFID tags of the container labels. Once a container is empty, it is simply placed in a collection box next to the shelf. The data is then automatically read from the RFID tags and transmitted to Böllhoff's ERP system. This process takes only a few seconds. Replacing the containers, including new RFID labels, installing the RFID antenna and commissioning the system all took place in a single day, in close cooperation with KTM. The existing shelf systems were left in place.



Inventory values reduced and demand fluctuations cushioned

Quick and easy to use, and ideal for managing fluctuating demand – KTM was impressed by the ECOSIT® RFID system. To such an extent that six months later the innovative RFID technology was introduced at the engine works too. The advantage is that no manual ordering is required. The delivery process then becomes considerably faster and more flexible. Even empty bins that were only read the day before supply can be replaced the next day. The risk of C-parts being unavailable is now all but ruled out, despite the marked seasonal fluctuations.

Customer benefits

  • Short response times
  • Reduced inventory value for customer
  • Better security of supply
  • Use of innovative RFID technology
  • Simple installation and start-up of system
  • Tidiness and order


Find out more: related downloads.

If you would like to know more, simply download the relevant brochures.

Title Language Version File Download
ECOSIT® ECOnomic Supply In Time
Economical procurement and distribution systems for fasteners
English 8500/16.02 2439 kB / PDF
English 8500/16.02 2439 kb / PDF

To view PDF documents, you will need the free Adobe Acrobat Reader.

More information

Would you like to discover more of the World of Joining?

Here you will find information about successful applications and related topics.