Press – 24.01.2017

PARRYPLUG® – Permanent protection against tampering


 

Stop! No unauthorised access!

A secure connection: PARRYPLUG® is a new development from Böllhoff to protect screw connections against unauthorised loosening. It is used where security is demanded and aesthetics required.

The innovation from the traditional company Böllhoff meets the growing demands for protection against tampering and theft in many technical areas. The locking element can only be removed with the help of a special tool. The PARRYPLUG® guarantees that only authorised persons and skilled personnel can access installations, machines and equipment. It is universal in use wherever the safety of both humans and machines is concerned and also the optimum prerequisite to prevent theft.

This product is made by Böllhoff

 

Nomen est Omen

The PARRYPLUG® (to parry – to ward off an attack) prevents the internal drive from being interfered with by tools using specially constructed axial ribs that assure a defined, secure press fit in the screw drive. Use of high-performance plastic allows for applications within a wide temperature range of ‑50 °C to +200 °C and the precision manufacturing assures that even smallest tolerances of hexagon socket drives can be considered.

Installation made easy

Mounting the PARRYPLUG® is extremely simple. Up to six plugs in the magazine allow for an effortless installation without tools. A handling aid enables mounting in the screw drive and then separates the plugs by rotating or tilting. All further plugs can now be installed without any additional preparations.

Security and customized appearance

While most fasteners perform their function hidden, the PARRYPLUG® is used in the exterior area and also meets aesthetic requirements. With the innovation in the sector of locking elements, the company Böllhoff provides an appealing technical design as the PARRYPLUG® can be coloured individually according to customer requirements and additionally protects the element from dirt and corrosion.

 

© Böllhoff Group, Bielefeld 2017

Reprint authorised.

 
 

Please send sample copy to

Bollhoff Inc.
Gretchen Kemsies
85 Royal Crest Court, Unit # 4
Markham, ON L3R 9X5
Canada

Downloads

For jounalists: related downloads.

If you would like to write about us, just download the press release and press photos.

What? File format / characters Release date Type / Size Download
Press text
.doc / 1,952 characters* January 2017 15 kB / ZIP
.doc / 1,952 characters* January 2017 15 kb / ZIP
Press text (short version)
.doc / 1,292 characters* January 2017 15 kB / ZIP
.doc / 1,292 characters* January 2017 15 kb / ZIP
Press photo (1)
.jpg / CMYK / 300 dpi January 2017 1146 kB / ZIP
.jpg / CMYK / 300 dpi January 2017 1146 kb / ZIP
Press photo (2)
.jpg / CMYK / 300 dpi January 2017 901 kB / ZIP
.jpg / CMYK / 300 dpi January 2017 901 kb / ZIP
Press photo (3)
.jpg / CMYK / 300 dpi January 2017 2191 kB / ZIP
.jpg / CMYK / 300 dpi January 2017 2191 kb / ZIP

* including blanks