Screws then become misaligned in the component (so-called “cross-threading”) and can jam. The result: damage to and even destruction of the holding thread. This can lead to manufacturing stoppages and considerable remedial costs.
Screws then become misaligned in the component (so-called “cross-threading”) and can jam. The result: damage to and even destruction of the holding thread. This can lead to manufacturing stoppages and considerable remedial costs.
The technical solution is as simple as it is ingenious. Developed originally for the automobile industry, NAVITIGHT® is now used in many other branches thanks to its outstanding properties. NAVITIGHT®’s secret can be found in the geometry of its thread run-out: the outer diameter of the narrower screw tip is smaller than the core diameter of the nut thread. The thread pitch, however, remains constant. When tightening the screw, the design brings the screw and nut into perfect alignment, ensuring that the screw fastening is completed correctly.
The optional additional paint removal function on the NAVITIGHT® screw will also help avoid other potential issues. In order to streamline processes, entire components are often painted in one go. This results in paint covering the thread which can lead to incorrect screw fastening. The NAVITIGHT® screw with paint-removal groove makes the internal thread viable once more as the groove scrapes the paint flakes from the thread.
The standard NAVITIGHT® screw has a hex flange head and comes in sizes M 5 to M 14. Other drive forms and dimensions are also possible.
Reprint authorised.
Frank Nientiedt
Head of Corporate Marketing
at Wilhelm Böllhoff GmbH & Co. KG
Telefon +49 521 4482-01
Telefax +49 521 449364
E-Mail presse@boellhoff.com
Bollhoff Inc.
Gretchen Kemsies
85 Royal Crest Court, Unit # 4
Markham, ON L3R 9X5
Canada
If you would like to write about us, just download the press release and press photos.
Title | Language | Version | File | Download | |||
---|---|---|---|---|---|---|---|
Press text
|
.doc / 1.869 characters* | January 2016 | 6123 kb / ZIP | ||||
Press photo (1)
|
.jpg / CMYK / 300 dpi | January 2016 | 2569 kb / ZIP | ||||
Press photo (2)
|
.jpg / CMYK / 300 dpi | January 2016 | 1614 kb / ZIP | ||||
Press photo (3)
|
.jpg / CMYK / 300 dpi | January 2016 | 1924 kb / ZIP |
* including blanks