Industry solutions

Zöllner Motors

Repairing with HELICOIL® Plus thread inserts reduces costs and saves time for the customer.

Repair instead of replace

With thread wear, there are two possibilities: either replace the entire component or repair it with our HELICOIL® Plus thread inserts.

Zöllner Motors has made a name for itself in Baden-Württemberg for cylinder grinding and motor repairs. Its good reputation lies in the inexpensive repairs offered to its customers. We contribute as well with our HELICOIL® Plus thread inserts.

Initial situation

 

Threads damaged by wear

Small detail, significant costs. In years gone by, it was often necessary to replace entire components, even though just one thread was worn - much to the dismay of the customer who had to bear the considerable costs. Therefore Reiner Bohlender, proprietor of Zöllner Motors, was looking for an alternative. For professional motor repairs in line with the current market value of the vehicle.

Customer profile

Industry
Cylinder grinding shop and motor repairs


Headquarters
Gerstetten / Germany

Solution

 

HELICOIL® Repair Solutions by Böllhoff

Nowadays many faulty threads can be repaired using HELICOIL® Plus thread inserts. The master mechanic drills the core hole first before cutting the right thread with the special HELICOIL® tap. The HELICOIL® thread insert is then screwed in using an installation mandrel – and the thread is good to go! With the HELICOIL® Plus Kit all necessary tools and parts are right at hand.

Result

 

Low cost, highly resilient

The thread is not only replaced, it is also even more resilient than before. For this reason, HELICOIL® Plus thread inserts are not just used for repairs: in fact, Zöllner Motors fits all threads being heavily stressed and in frequent use with HELICOIL® thread inserts as a preventative measure.
Typical problem scenarios in cars include oil drain, spark plug and lambda probe threads as well as repairs to the wheel bearing. For such cases, we supply special HELICOIL® Plus Kits tailored to the respective requirements.

Customer benefits

  • Quick and inexpensive repair
  • Highly resilient thread

Downloads

Find out more: related downloads.

If you would like to know more, simply download the relevant brochures.

Title Language Version File Download

To view PDF documents, you will need the free Adobe Acrobat Reader.

More information

Would you like to discover more of the World of Joining?

Here you will find information about successful applications and related topics.