Success stories

Pkw-Service Hartinger

Repair car threads quickly and cost-effectively. With RIVKLE® Plus Kit for resilient joints.

For load-bearing threads

Resilience is an essential requirement of threads on vehicles. By means of Böllhoff Repair Solutions, thin-walled components can be provided quickly and economically with load-bearing threads.

Pkw-Service Hartinger in Gerlenhofen, Germany, keeps our blue HELICOIL® Plus Kits permanently in stock. That’s how Bernd Hartinger, trained master mechanic and general manager, came across RIVKLE® Plus. Ever since using them for the first time, he has relied on the load-bearing blind rivet nuts from our repair range.

Initial situation

 

Repair cases

If it’s worth repairing, it’s worth doing right. A typical repair for Pkw-Service Hartinger is mounting a thread to the car metal for attaching the numberplate. Conventional tapping screws are often not strong enough. Defective threads in motorcycle frames are also common problems in the car shop, for example, when attaching the luggage rack. Aluminium blind rivet nuts are usually used for this purpose; however, they are less resilient to heavy loads.

Customer profile

Industry
Car shop

Headquarters
Gerlenhofen / Germany

Established
2007

Solution

 

RIVKLE® Repair

RIVKLE® blind rivet nuts create internal threads on thin-walled components.
For hollow sections, profiles, housings and other parts that permit access from only one side, the insertion of a blind rivet nut is often the only solution. The same is true when it comes to attaching numberplates and luggage racks.
The RIVKLE® Plus Kit consists of a hand tool and the respective RIVKLE® Plus blind rivet nuts of the desired size. As with every Böllhoff Repair Solution, all the required tools and components are included in the RIVKLE® Plus Kit.

Result

 

High thread stability

Repaired and improved. Fitting a steel RIVKLE® Plus blind rivet nut makes the thread more stable. The joints are even more resilient than from the factory.

Customer benefits

  • Quick and inexpensive repair
  • Load-bearing thread on thin-walled components
  • Assembly with access from only one side ("blind"),
    even on hollow profiles
  • Screws can be inserted multiple times
  • No rework necessary, even with pre-coated parts
  • Small countersunk head for small head projection (no need to countersink the workpiece)

Downloads

Find out more: related downloads.

If you would like to know more, simply download the relevant brochures.

Title Language Version File Download
Car repair solutions
English 0195/15.02 931 kB / PDF
English 0195/15.02 931 kb / PDF
Door module
Innovative joint solutions for the door module
English 0941/15.02 1302 kB / PDF
English 0941/15.02 1302 kb / PDF
Innovative joint solutions for the front and rear end module
English 0942/17.02 3869 kB / PDF
English 0942/17.02 3869 kb / PDF
Lightweight construction
Efficient joint solutions for lightweight construction
English 0949/16.02 1085 kB / PDF
English 0949/16.02 1085 kb / PDF

To view PDF documents, you will need the free Adobe Acrobat Reader.

More information

Would you like to discover more of the World of Joining?

Here you will find information about successful applications and related topics.