05.05.2010
Efficient combination of driving features
The Torx- or hexalobular internal driving feature has long taken as an efficient driving standard in the production.
But there are also applications, where it is not used so far. This is especially the case if the connection has to be released again because of maintenance or repairs reasons.
The arguments that engineers do not always have tools for hexalobular internal driving features available, or the internal drive due to dirt is no longer usable, then prevent an economical initial assembly.
So why not combine the two applications?
How such a screw could look like, you can see in the picture. Further drive form combinations, screw geometries, different thread forms, surfaces, etc. are possible. We would be glad to inform you about your options.