Automotive & aerospace
Car gear box cover made of aluminium die-cast,
HELICOIL® plus, M 14 x 1,5 x 14, free running
For use in gear boxes, exhaust systems, engines and satellites, for thread reinforcement, repeated screwing, maintenance and repair
Thread inserts
HELICOIL® thread inserts create high-strength fastenings in metal low-strength materials and have been well established on the market for about 50 years.
Function
HELICOIL® plus thread inserts create high-strength, wear-resistant, heat-resistant threads of highest precision. They are available in free running and screwlock version. The green or red colour allows easier identification when they are installed.
Benefits
HELICOIL® thread inserts are available with imperial or metric dimensions and as special designs.
The newest generation of this technology is HELICOIL® plus. Easy handling
allows easier installation. Thanks to the reduced diameter in the first thread, the thread insert can be screwed in like a screw.
HELICOIL® plus inserts are highly wear-, corrosion-, and heat-resistant and show low thread friction within small tolerances.
The thread insert with precision formed, rhombic profile is available as free running or screwlock version.
Our seal of quality, a rhombic imprint at the end of the last thread, unmistakably identifies each Böllhoff HELICOIL® plus thread insert as an original.
In contrast to the HELICOIL® plus, the HELICOIL® tangless does not need a tang. This results in a reduced assembly time. A tang breaker is not required. The HELICOIL® tangless is used in applications in which tang removal must be executed with high reliability for reasons of safety.
The HELICOIL® tangless is compatible to the HELICOIL® plus system. This means:
The HELICOIL® tangless is available as free running and screwlock version.
Is the tapped hole widely torn?
Has the thread been cut too large?
For these cases the HELICOIL® plus TWINSERT is the ideal repair element.
HELICOIL® plus TWINSERT consists of two HELICOIL® plus thread inserts. The external element is a HELICOIL® plus free running. For the internal insert you can choose between HELICOIL® plus free running and HELICOIL® plus screwlock.
Every thread of the thread insert with precision formed, rhombic profile is free running. The result is an internal thread true to gauge that can be used on both sides.
The green colour allows easier identification when the HELICOIL® plus free running is installed.
Our seal of quality, a rhombic imprint at the end of the last thread, unmistakably identifies each Böllhoff HELICOIL® plus free running as an original Böllhoff product.
The HELICOIL® plus screwlock bears the same benefits regarding threads as the HELICOIL® plus free running.
In addition, an integrated screw-locking area serves as a screw lock.
Locking of the screw is achieved by one or several polygonal-shaped threads that clamp the flanks of the screwed-in screw. The result is an elastically resilient frictional locking.
The HELICOIL® plus screwlock can be recognised thanks to its red colour.
The HELICOIL® screwlock inserts can only be used with screws of property class 8.8 or higher.
Car gear box cover made of aluminium die-cast,
HELICOIL® plus, M 14 x 1,5 x 14, free running
For use in gear boxes, exhaust systems, engines and satellites, for thread reinforcement, repeated screwing, maintenance and repair
Carrier plate for electronic components made of aluminium pressure die-casting
For use in lamps, electrical appliances, drill hammers, etc.
Machine construction console ,
Material G-AISi9 Mg,
HELICOIL® plus, M 8 x 12,
free running
For use in printing presses, in high temperature range, for repeated screwings, maintenance and repair
If you are not able to open the document, please install the Adobe Acrobat Reader.
Copyright © 2010 Bollhoff Fastenings Pvt. Ltd.