09.09.2011
HELICOIL® repair pack M 9 x 10 now available!
Wheel bearing housings are constantly exposed to a variety of different loads, with wear as the the logical consequence. For example, the internal thread, cut in the wheel bearing housing and used to screw in the brake guide bolts, is often damaged during the disassembly of those guide bolts.
A damaged thread usually requires replacement of the complete wheel bearing housing.
Böllhoff offers an alternative solution with the new HELICOIL® repair pack for wheel bearing housings.
The repairing is simple and occurs in one manufacturing step by a combined drilling and cutting tool before the HELICOIL® is turned into the new thread by the means of an installation mandrel.
Repair solutions with the proven HELICOIL® technology, which reduce time and costs.
The repair pack is approved by the TÜV (on selected wheel bearing housings).
For any queries, please do not hesitate to contact us
- Telephone +49 (0)5 21 / 44 82 - 05 (2 34)
- Contact form