Certified testing laboratory

  1. Böllhoff Austria >
  2. Services >
  3. Certified testing laboratory

Certified testing laboratory

The accredited test laboratory at Böllhoff offers a complete range of services involved in the destructive testing of fasteners of all types.

The test laboratory performs research and testing principally for Böllhoff Group companies. It will also undertake commissions for outside companies.

Services

The modern, fully equipped laboratory staffed by expert personnel will perform mechanical-technical, physical, chemical and metallographic testing. Tests are performed for the following areas:

  • Quality assurance
  • Customer-specific tests
  • Product development
  • Prototype testing, defect and damage investigations, complaints
  • Assistance and consultancy to members of the Böllhoff Group and their customers providing expertise in materials and testing.

Mechanical-technical testing

  • Tensile strength and compression testing to 400 kNHardness testing
  • Screwing tests (torque, angle of rotation, preload force)
  • Adhesion factor analysis
  • Structural testing, metallography
  • Surface defect inspection
  • Sealing tests
  • Cleanliness testing
  • Vibration testing of fasteners up to M16 size
  • Continuous vibration testing up to 150 kN ± 75kN

Physical tests

  • Coating thickness measurement - X-ray fluorescence analysis
  • Optical emission spectroscopy

Chemical testing

  • Corrosion testing (salt spray mist, Strauss test)
  • Chrome VI content testing of surface coatings

Preparation of mechanical samples / Preparation / Test rig and equipment

Download Version Language Type/Size
Service offer January 2012 English PDF / 2.604 KB

If you are not able to open the document, please install the Adobe Acrobat Reader.



Böllhoff is certified

Here, you find out in which fields!

Certificates & standards

Jobs & career

Looking for information on jobs & career?

Jobs & career

Contact

You need any product information or support?

Contact

A view into the testing laboratory

  • A view into the testing laboratory – Receipt of laboratory orders

    Receipt of laboratory orders

  • A view into the testing laboratory – Tensile test of screws

    Tensile test of screws

  • A view into the testing laboratory – Checking of the microstructure at the light microscope

    Checking of the microstructure at the light microscope

  • A view into the testing laboratory – Determination of the friction coefficient at the screwing test bench

    Determination of the friction coefficient at the screwing test bench

  • A view into the testing laboratory – High frequency vibration fatigue testing machine for testing of the fatigue strength of fasteners

    High frequency vibration fatigue testing machine for testing of the fatigue strength of fasteners

  • A view into the testing laboratory – Detection of Chromate in coatings

    Detection of Chromate in coatings

  • A view into the testing laboratory – Salt spray test

    Salt spray test

  • A view into the testing laboratory – Visual test of surfaces at the 3-D-microscope

    Visual test of surfaces at the 3-D-microscope

  • A view into the testing laboratory – Area of the mechanical technological tests

    Area of the mechanical technological tests

  • A view into the testing laboratory – Thickness measurement of coatings and material analysis

    Thickness measurement of coatings and material analysis

  • A view into the testing laboratory – Tensile tests and screwing tests

    Tensile tests and screwing tests

BÖLLHOFF

Copyright © 2011 Böllhoff GmbH