2 in 1

Easier maintanance + lower assembly costs

  1. Böllhoff Austria >
  2. Company >
  3. News & press >
  4. News >
  5. 2 in 1: Easier maintanance + lower assembly costs

21.12.2010

Efficient combination of driving features – FLEXIDRIVE®

The Torx- or hexalobular internal driving feature has long taken as an efficient driving standard in the production.

But there are also applications, where it is not used so far. This is especially the case if the connection has to be released again because of maintenance or repairs reasons.

The arguments that engineers do not always have tools for hexalobular internal driving features available, or the internal drive due to dirt is no longer usable, then prevent an economical initial assembly.

So why not combine the two applications?

How such a screw could look like, you can see in the picture. Further drive form combinations, screw geometries, different thread forms, surfaces, etc. are possible. We would be glad to inform you about your options.

Please send us an e-mail to fastenerservicesupply@boellhoff.com.



Product catalogues

You need further technical information?

Download centre

Jobs & career

Looking for information on jobs & career?

Jobs & career

Contact

You need any product information or support?

Contact

2 in 1

  • Efficient drive combinations FLEXIDRIVE®

BÖLLHOFF

Copyright © 2011 Böllhoff GmbH